I want to get continusous power supply for my load. I use a 12V DC Fan connect to VSYS and PGND to test.
use 3S lion battery and short 4P and 4N.
use a 19V,3A power supply on VAC and PGND.
connect EV2400 on SMB bus.
use defalut firmware,download from web site (sluc598.zip).
after the connections , push the wake-up button, the bqstudio look ok. battery voltage,AC power are ok. bus the fan don't work .
I can use the COMMAND button control the discharge and charge.
Now,I want to a cotinusous power supply.
1.only battery,then battery discharge. VSYS output.
2.VAC=19V,then battery can be charged automatic. if battery is full,charge stop automatic.
3.only VAC=19V.then VSYS output.
so,What should I do?
The default firmware is ok? I need the learn cycle? need the calibration?
Thanks!!!