Hello,
I've just finished a design using the BQ76920 + external uC for a 5S battery and brought it to small production level. Through all prototype stages, we were very happy with the results. On assembling our first production run, we've found that if the assembly connects the BATT+ & BATT- lines, the BQ76920 immediately overheats and smokes out, destroying the IC. If the cell lines are connected at the same time or in ascending order, this behavior is not yet encountered (approx. 100 devices tested).
Is this to be expected in any way or is this indicative of a design flaw? For what it's worth, the design is exceptionally close to examples from the EVM & datasheet.
Please let me know if there is any set recommendation for assembly order of packs using the BQ76920 and whether or not this is a known behavior which must be accounted for at the assembly stage. Production is on-hold until we have this issue resolved, so any prompt guidance is greatly appreciated.
Thanks.