The TPS2066 Enable pins (EN1 & EN2) are active high. If I want to permanently enable the outputs I would pull these pins high to 5V. In this case should I use a pull-up resistor i.e. 10kohm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TPS2066 Enable pins (EN1 & EN2) are active high. If I want to permanently enable the outputs I would pull these pins high to 5V. In this case should I use a pull-up resistor i.e. 10kohm?
Hi Mark,
This part falls under the Power Interface forum. I will go ahead and move this post.
Thanks,
Alek Kaknevicius