This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133 Charge Fault [Urgent]

Other Parts Discussed in Thread: BQ24133, BQ3055

Hi,

We have designed a battery charging circuit based on BQ24133 Charger IC in the initial version board works well and it has few layout mistakes i corrected and done second revision board, but the second revision board the moment i turn on the charger the fault status LED starts blinking, can any one help me to fix this.

Here is my Input and other conditions

Charge Input Voltage: 15V @1.5A

Charger current (Iset) : 1A

ACSet: 1.4A

TTC Set:  Pulled low

Thermistor: 103AT

Number of Cells: 3 (each 4.2V @2500mAh

Voltage measured when fault LED blinking 

VBAT: 10.26V

SRN: 10.26V

SRP: 10.26V

VISET: 0.2V

VTherm: 2.09V

VACSET: 0.54

TTC: 0V

Vref: 3.3V

Vregn: 5.95V

VACP & VAC: 15.09V

VACDRV: 20V

VCMSRC: 14.7V

voltage between BTST to SW pin am getting only 300mV but as per the datasheet it should be min 4V to charge i haven't got any reason why it is in 300mV and SW pin is in DC level there is no switching happening, and at this condition it takes only 6mA current from my charge input,

i have attached my schematic here, battery ground and charger IC ground are connected through 10m ohms sense resistor to monitor battery charger which is connected in BQ3055 battery gauge