This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is my .srec ready for Golden Master?

Hi,

4s1p, Honcell HCP487390, 3.7V, 3900mAh, 14,43Wh.

v13, build 19.

.srec attached.

Do you see an oversight on my side?

Thanks,

Ivo

5141.v13.zip

  • hi Ivo,
    What device are you using? As long as you have a learning cycle successfully complete.. update status will be 06 for pack side gauges and 02 for system side gauge if learning was successful, you should be okay. You will need to change cycle count to 0. Also, manually change update status from 06 to 02 if using a pack side gauge.

    thanks
    Onyx