This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25121 Reset and OTP

Other Parts Discussed in Thread: BQ25121

Hi,

We were designing a wearable with BQ25121. The device outputs 2.5V at startup and is then programmed to 3.0V on the run.

In case we reset the device with MR#, or the device gets down when the battery is completely drained, does the device needs to be re-programmed to output 3V on next power up/ start up after reset?. In datasheet, was the default OTP setting refer to default register setting to 2.5V, that is programmed at factory?..Please let us know

  • Kavin,

    I believe there is some confusion on the reset function. The reset through /MR pin will pull-down the Reset line which if connected to your MCU, will cause it to reset. We will hold the value until altered over I2C. It is not a reset to our device but a reset to your MCU if desired. Yes the 2.5V is programmed at our factory.


    Regards,
    Gautham
  • Hi Gautham,

    Thanks for the clarification.

    Can you let us know the occurrences when the I2C register setting for desired output (3.0V) rather than factory programmed setting, will be lost.

    Regards

    kavin