Other Parts Discussed in Thread: TPS55330
Hi,
I use the online tool (see attached pdf) to design a 9V to 12V boost converter with TPS55330. The output of the converter is connected to a solenoid, which draws 1A when activated. When solenoid is fired, the output of the converter drops from 12V to 8V and there is oscillation every 1.3us (see attachment). I can also hear a high pitch noise while the solenoid is fired.
Where should I start to solve this issue?
Thanks,
Philip