Hi All
I am facing problem in charging battery by BQ24297EVM-021.
Hardware configurations are :
Connected a 5V DC 2.1 A charger on J7
Battery ( 3.7V 2100 mAh) with ammeter in series on J2 ( BAT+ & GND).
INSTALLED : JP3,TS2,TS1,JP5,JP7 , JP2 : D- and D-/PG shorted & JP10 : TS2-I & TS2 shorted.
NOT INSTALLED : JP6,JP1,J5,J6,JP4.
R15 = 135 Ohm.
Software configuration:
I am configuring register as shown in image :
Problem :
According to the configuration battery should be charged by 1024mA but it is not getting charged (Ammeter reading is in negative micro ampere).
And after few seconds the configuration changes automatically ( as shown in below image), & ammeter displays +171 mA .
Please guide me through this.
Thank you !
Regards
Kunal