As the subject line states we are looking for some recommendations for a high power DC/DC converter with the following parameters:
Vin: 32 – 48 VDC
Vout: 12 VDC
Iout: 250 A
The application this is to be designed for has a maximum up time around 10 minutes, and will be shutdown for the majority of the time. We are looking at doing a multiple phase design due to the high current requirement but can’t seem to find any TI products that fit our needs. In case we missed something I wanted to post on here for feedback.
Thanks!
Dave Kaplin