This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Undershoot of TPS61087

Other Parts Discussed in Thread: TPS61087

Hi

My customer evaluates TPS61087 using EVM under the following conditions.
But switching voltage's undershoot is -0.82V, so the value is over the Absolute Maximum Ratings of this device.
Could they use it this condition?
If it is bad, could you tell me the solutions?

Conditions
  Vin=4.1V
  Vout=5V
  Iout=No Load
  fsw=1.2MHz

Best regards,

Yokota