My target is to make 5V / 1000mA max with 3 NiMH batteries. The TPS61230 looks very good to make this function.
I adjust the input hysteresis with Vin_off = 2.51V and Vin_on = 3.63V (for reference in the datasheet it's REN1 = 1000k, REN2 = 487k and REN3 = 348k).
The output is normaly at 850mA, so the NiMH current is big. When the 3 batteries are under 2.5V, the TPS61230 switch off. When the ouput current is #0 when the TPS61230 is off, the volatge of the 3 batteries increase more than 3.70V, so the TPS61230 restart but the NiMH voltage fall quickly and the TPS61230 switch off.
If I increase the Vin_on, I affraid the TPS61230 will never start when the 3 batteries are a bit low.
What is your recommandation about this problem ?