Hi,
I have built a PMP11282 Rev A Evaluation board in order to asses the interleaved/boost LLC combination. The interleaved boost works fine but I'm having some issues with the LLC.
The LLC runs but if I turn it on into a load (say 10A or more) or I do a large load change (say 2A to 12V) it blows the half bridge fets and the UCC27714 Hi/Lo Side Gate driver chip. The circuit has been built as per the documentation. The only change that I've had to do is with the resonant capacitor (C519). I couldn't get the part recommended in the BOM as it was out of stock so I've used four (4) 47nF/1000V ceramic capcitors with two sets of 2 capacitors in parallel placed in series to give me the required 47nF value (I did it this way as I has some problems with the ceramic capacitor flashing over during turn on when I only had a single 47nF/1000V capacitor).
If anyone has any suggestions as to why this might be occuring I'd appreciate it.
Thanks for your help.
Regards,
Gareth