Hi,
we are using LM5085MY IC in our power supply design. (Input 55-64V) and output -41VDC,5A) . while doing temperature rise test, we observed IC heats up to 100 degree centigrade in 15 minutes if we load the output to 1.5A. Attached schematic and layout of IC for reference. Output current requirement is upto 6.5A but even with 1.5A, IC is heating this much so we are not sure about temperature rise at 6.5A output.
Please advise to resolve this heating issue.
Thanks,
smitha R