This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Synchronizing two LM5175

Other Parts Discussed in Thread: LM5175

Hello

What is the best way to synchronize frequency of  two lm5175 controllers? The best if one from another.

Regards

Miro

AFAE

  • Hi Miroslaw,

    The best way is to use an external synchronization source and ac-couple to the RT pins of the LM5175s. The external synchronization frequency should be 110% or higher of the RT programmed setting.

    Another way could be to use the drive or SW pins to generate SYNC out. It is complicated by the fact that the switching pattern in buck, boost, and buck-boost are different.

    Thanks and regards,

    Vijay