We are working on a POS device protoype
We have to use Fuel Gauge in our system to detect the below battery properties,
1. Current Battery status in percentage not in volts.
2. Current Battery charge state(Charging/Not charging)
3. Alert system when battery percentage is less than 15%.
and we are planning to use TI's BQ34Z100-g to accomplish the above tasks.
I would like to know the Registers/commands that we can use in Application to get the above details.
I read datasheet but not sure got what I need. As I need to finish off this task. some help from here will be good.
Thanks in Advance
Sarjoon.