I want to use two of these devices in parallel battery packs. Can I change the Address one of the devices?
If not, How hard is it to compile a new firmware with that very simple change?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use two of these devices in parallel battery packs. Can I change the Address one of the devices?
If not, How hard is it to compile a new firmware with that very simple change?
Sean
The bq34z653 is the only other device that has the heater control option, but its SMBus address is fixed as well. You may be able to use an SMBus multiplexer to add more than one of the bq34z651 devices to the bus.
Tom