Hello,
Can I use the LM1084 when I set the adjustable output voltage to 19V and my nominal input is 14.4V. Load current is 2A.
I'm only adding the regulator for when a user uses a larger battery, which is rated at 20V max. In this case there will be some heat generated as the power dissipation will reach ( 20V-19V = 1V * 2 A = 2W )
Are there any cons in using the LM1084 regulator is set to 19V and the input voltage is lower? Or are there better ways of doing this?
Thanks