Hi
I am designing multi-rail type power supply for microprocessor based system. It includes supply like 1.2V 0.85A (For Core), 3.3V 0.9A (For I/Os and peripheral) and system will operate on 400MHz clock signal. Which regulator is to be used for this type of application linear or switching . What all parameters I should consider while selecting regulator (except efficiency).
I got two IC in power management section one is linear regulator (TPS 70302) and other one is switching regulator ( TPS65023) . Please suggest which one is best?