This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bq78PL116 issues; short circuit & capacity

Other Parts Discussed in Thread: BQ78PL116
1. Bq78PL116 not able to detect short circuit condition. I have 1miiliohm sense connected & used "Hardware Short Circuit Threshold = 37" i.e minium value for short circuit protection. I have passed current upto 80A for long duration i.e 5 sec or more but pl116 never detect short circuit protection.THough OCD1 & OCD2 works fine always never have issue in it. Part is calibrated for current.
2. Second problem is I have 7S60P configuration. EVM says number of parallel cells can be set my .tmap file.
But its utility only allow for max 32 paralle cells. How to enter exact capacity of 60P * 2600mAH in configuration.
ATtached find its saved parameter files.

bq78pl116.zip