This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is UCC28740 certified by UL

Other Parts Discussed in Thread: UCC28740

Dear,

We are using UCC28740 in our AC-to-DC module, the design is base on one of TI reference design, please review attachment for more detail.

I would like to know that if the UCC28740 is certified by Underwriters Laboratories (UL) as apart of power supply safety standards.

Thanks,
Hoang1234.AC-DC 5V-3A.pdf

  • Hi Hoang,

    In general the power supply controller does not require UL approvals as the controller does not cross the isolation barrier like the transformer or opto-coupler.

    Is the customer looking for UL information relating to the device?

    Regards

    Peter