Hello,
I'm looking for a simple way to provide a good power supply for an audio circuit. It is USB powered and uses a 98dB SNR DAC so I'd like to stay at that range for the audio stage. I need to generate a +15V and -15V supply and I was looking at the TPS65130/1 as a nice all in one chip. It's stated as good for display biasing and such but I was wondering how good the output is for audio op amp control. This will mean a lot of transient current demand and some slight input voltage change depending on the quality of the USB host port. If I filter the output well and provide lots of capacitance to keep the ripple low, do you think I will have any issues with noise leaking into my audio stage? Any recommendations for such a case? I don't expect to use more than 100mA on each rail as worst case peak with normal usage under 50mA on each rail.
Thanks!