This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5433

Other Parts Discussed in Thread: TPS54332

Hi,

I am using TPS5433 to convert power to 4 volts, 2Amp. As per my understanding  no matter what is inpt voltage between 3.5V to 28V my output voltage will be 4V when I configure output voltage to be 4V...Am I right??

But while testing I noticed output is going low to 2.7V when I connect input to 5.5V. 

Output is 4V anything above 5.5V and goes low to 2.7V as soon as I decreas input to 5.4V.

Please suggest me how can I make input range of 3.5V to 28V to be valid.

Regards

Bharati