This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB to GPIO interface update required for Pl114

Other Parts Discussed in Thread: BQWIZARD

Dear TI help,

Reading several threads in this forum I am running in the same problems to perform the required update of the USB to GPIO interface for operation with the Pl114.

I can not update the USB to GPIO via bqwizard, since the update text file from brqwizard refers to menus that do not exist. (I have installed v 2.5.7).

I also cannot update via the "USB-to-GPIO firmware loader" tool: where are the required bin files to be found?

Generally: I do not seem to get connection (but the green led is on).

Q1: Where are the bin files to update the USB to GPIO so it can work with the PL114?

Q2: How to finish update of the USB-to-GPIO as well as PL114 EVM?

 

Note: This Bqwizard software is crashing awfully frequently, BTW.