This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

240W,10A Power supply Design

Other Parts Discussed in Thread: UCC28063, UCC28180, UCC25600

Hi,

I want to design a power supply with 24V DC,10A current from 240V AC supply.Do you have any solutions for this? or kindly suggest me some power controller ICs to make it happen? 

  • Hi

    At 24Vdc, 10A we would recommend an LLC stage, UCC25600. At this power level you may also require a PFC front end to meet AC line current harmonic regulations, the UCC28180 is a good solution as is the UCC28063 device if you need the design to fit nto a low profile space like DTV.

    If you go to the webpages for these devices you will see reference designs that may be of interest for you.

    Regards

    Peter