HI all,
I have a project where the capacity is relatively small - 5Ah but max continuous currents can reach 50-60A.
I want to use all layers of current protection, meaning both hardware and standard.
that means I need to scale the current reading because max value for current reading is -32.768A,
this way I will have OCD1 and OCD2 in use as well.
what will be a better method for me, to use IP scaling or calibrate the sense resistor to divide the current?
- I'm worried that capacity calculations will be not accurate enough because of the small resolution in measurements, will it?
- do you have a better idea for parameter set up for this case?
Regards,