This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54540 Vout dropping down to zero on loading



Dear friend,

Vin = V_EN = 15V

Vout = 12V

When there is no load, output voltage is 12V, but when loading the output to 5 ohm the voltage is dropping down.

P01_LED.pdflease see attached scheme. Do you have any suggestion why its happen?

*Design circuit according to WEBENCH.

Thank you,

Ron.