Hi,
I have a question concerning the BQ76930 battery monitor and balancer:
We have two times 4 Li cells, which we connect either in series (making it 8 cells) or in parallel (making it 4 big cells). This will be switched over during operation. Is it possible to use the BQ76930 for this application? I would connect the first 4 cells to VC0 to VC4 and the second 4 cells to VC5b to VC9. Will this create problems when the Cells are connected in parallel, so VC5b will be at the same GND potential as VC0?
Thanks for your advice,
M. Schmid