Hi,
Customer would like to use TLV62084 under below condition. From webench, we proposed 1uF and 22uF output cap. Now customer prefer to use 0.47uH. is it ok for them? What is the suggested output cap value? Is 88uF ok for them? THanks!
- VIN: 3~4.8V
- VOUT: 0.55V~1V
- IOUT: 2A.
Antony