Hi all.
I would like to get accutual effiency data.
The input and output condition is the following .
TPS62090 and TLV62090 efficiency comparison
■Test condition 1
Input 3.3V
Output 1.2V / 0A~2A
■Test condition 2
Input 3.3V
Outut 1.5V / 0A~2A
My customer expects that two device efficiency are same result.
Brst Regards,
Sho