Dear Sir
May we have PMIC can dynamic adjust 4 outputs(power sequence/enable/Vout voltage ) by I2C or SPI for SSD application?
Vin is 5V Vout is adjustable and output current is 4A/3A/3A/3A. like ACT8870.
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
May we have PMIC can dynamic adjust 4 outputs(power sequence/enable/Vout voltage ) by I2C or SPI for SSD application?
Vin is 5V Vout is adjustable and output current is 4A/3A/3A/3A. like ACT8870.
Bogey
Hello,
You could check http://www.ti.com/product/LP8758-E0 is that suitable for the application. Can you tell more details about the use case, average currents etc.?
Thanks.
Best Regards,
Tomi Koskela
Hi Sir
The customer want use I2C(or SPI) to control output voltage after power on. for example, here after power on that buck1 =1V/buck2 = 1.8V/buck3=3.3V buck4=2.5V.
and some condition they want to dynamic control let buck1 = 1.5V/turn off buck 2/ buck 3=2.8V/ buck4 =2V. and customer also help can control power sequence by dynamic.
Bogey
Hello,
Ok, sounds like LP8758-E0 would be a good fit for this. It allows enabling/disabling outputs/changing the voltage level with gpio pins as well as with I2C registers.
Thanks.
Best Regards,
Tomi Koskela