This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question on selecting the correct ChemID from a list obtain from GPC tool

I recently submitted the data to the GPC tool for a relative low capacity cell rating at 950mAh.

The list of ChemID I got back from the GPC tool seems to have quite a wide ranging capacity

as high as 7000mAh.  Interestingly, the best match ID 1356 has one of the highest

capacity rating at 6200mAh.  The closest match in term of capacity and % is chemID 148 which is 900mAh.

So my question is which ChemID should I select? 

Below is a list of ID returned from the GPC tool. 

Thanks.

Chem ID    max DOD error, %    Max R deviation, ratio
1356    1.05    0.13
116    1.11    0.76
148    1.12    0.79
469    1.16    1.93
2118    1.16    1.93
1328    1.42    1.35
1344    1.46    0.15
1345    1.47    0.12
1362    1.51    0.15
1327    1.6    0.21
1363    1.63    0.66
1361    1.69    0.03
120    1.73    0.8
1287    1.81    0.24
1116    2.17    1.54
1208    2.26    1.52
1336    2.35    1.51
149    2.37    0.88
129    2.47    1.93
1334    2.52    1.82
172    2.56    1.95
125    2.59    1.06
128    2.6    0.88
180    2.85    0.8
126    2.88    0.99

  • Andy
    The capacity listed with the ChemID was the cell that was characterized. Capacity is not stored in the chemistry data and a good OCV match is the most important factor. I would use the ChemID listed with the lowest OCV error.
    Tom