Dear Ti,
I'm looking to use the TPS54360 as my specs are as below.
Vin=48V
Vout=3.3V or 5V
Iout=<1A
After I had done a simulation through Webench found that the efficiency only achievable at +/- 70%. Please check and advise.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti,
I'm looking to use the TPS54360 as my specs are as below.
Vin=48V
Vout=3.3V or 5V
Iout=<1A
After I had done a simulation through Webench found that the efficiency only achievable at +/- 70%. Please check and advise.
I ran a webench simulation and set output to 5 V at 3.5 A and set the optimize dial to "max efficiency". The efficiency at 1A output is greater than 91%:
Designing for max current will usually result in highest efficiency at lighter loads. Mainly due to lower DCR of inductor. Also, 5V output will always give better efficiency than 3.3 V. If you provide your email, I can share the actual webench file.