This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Potting/ encapsulation of BQ2060A issues

Other Parts Discussed in Thread: BQ2060A

Hello,

Has anyone experienced issue with the gas gage BQ2060A after the component and board were being potted?

I used potting material Hysol e-60 (10Mohm insulation resistance).

I have several boards being defective (no more led status displayed) after the potting was done (cured at room temperature for 24H).

I am wondering if the potting material would interference with the BQ2060A high impedance input up to the point of damaging the component.

Thank you

Regards,

Frederic P