Hello.
My customer is currently in using TPS62560,now.
I have gotten a question about this product .
So, please teach me about TPS62560.
<Question>
If EN PIN is a case where rises earlier than the VIN PIN, is there a possibility that output voltage is latch at 0V?
(Yes or No?)
<Comments>
Of course, my customer knows that this device's EN PIN Absolute maximum Rating is "-0.3 ~ VIN +0.3, ≤ 7" .
So, the customer has formed a circuit with VIN = EN.
But, in the wiring length influence, have to worry about if EN get up earlier than VIN.
So , please tell me .
Best Regards,
Masumi Sekiguchi