This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2674 External power feed parallel to output

Other Parts Discussed in Thread: LM2674

We  have been using the LM2674 in a standard application where feed voltage (+VP) is 24VDC and output (+12V) is 12VDC at 300mA.  See included schematic.  We are looking at using the same circuit board but in an application where the input (+VP) to this regulator will not be connected and the output (+12V) will have a alternate 12VDC source connected in parallel.  We have tried this on the bench and everything appears to work OK but I do not have a detailed schematic of the internals to the LM2674 to confirm.

Would like to know if the LM2674 will live quietly under this condition?

I do not mind if the part is damaged as long as it does not become a current sink.

Thanks for your help,

Gregg

  • Referring to the block diagram we see the power MOSFET connected from the VIN pin to the VSW pin. 

    This FET has a diode from VIN to VSW (cathode at VIN).  This diode will be forward biased if a voltage is present

    at VOUT and the input is floating or shorted to ground; the path will be through the inductor.  This may cause trouble in your

    system.  Also, a current flow through this diode may damage the LM2674.

    Therefore, we cannot recommend this type of operation.

    If possible some kind of diode-OR should be used on the output.