This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25011 burns after 2-3 minutes (and it works fine during those 3 muinutes)

Hi everyone

I have some trouble with this component. I use it for 5 years and never had problem with it.

Since few weeks, The component burns after 2-3 minutes of working. I only mount the regulator on the board (and the components around it of course).

It is the same PCB, same schématics . The self is a 22uH, 10uF for Cout. I have 12v IN and 3v3 OUT. Rsense 82mOhm, but I only need 200mA when the board is completely soldered. I had no problem with the 10 first new pcb, and now I can't have a working regultation... Does anyone have an idea about what happen on my board ?

A problem when I soldered the component ?

thank in advance

best regards

Sullivan