Hi,
I am trying to control 5 W (400mA * 10 V ) LED load using TPS2379EVM-106 through a an LED Driver circuit. But the load which worked fine independently with the driver circuit powered by 30 V DC, started to flicker when connected through TPS2379EVM-106. Can you please help us on the possibilities of troubleshooting this?Thank You.
Regards,
Gaayathri