Hello,
My customer have a question about OCP of TPS54427.
In the section 7.3.4 Current Protection(Datasheet P8),
It is written with [If the overcurrent condition exists for 7 consecutive switching cycles, the internal
OCL threshold is set to a lower level, reducing the available output current].
My understanding is that [After the over-current limit, current flows.], am I correct with this?
In addition, when the current is flowing, What is the range of the current?
And,Why current continues to flow?
(Does it flow in what route?)
Best Regards,
-Watanabe