[ LMG3410 ] Low Fs Operation and UVLO Behavior
Hi,
My customer has been studying GaN solution, e.g. LMG3410 for their AC servo motor application. Can you help me to answer some queries from them?
<Q1: Low Fs Operation>:
As my understanding, in general, GaN can offer more benefit on high speed opeartion such as MHz. However, my customer would like to use this with switching frequency as low as 7KHz range. Are there any negative point and/or drawback expected?
<Q2: VDD Supply Current For Low Fs>:
Do you have a graph which express VDD supply current down to few KHz? Fig. 5 in the datasheet show down to 10KHz.
(It's already close to 1mA, quite small, though.)
<Q3: UVLO Behavior>:
According to datasheet, UVLO is triggered with supply voltage lower than 8.6V (min). Do you have any data which show until how much low voltage can LMG3410 maintain its operation correctly?
Thank you for your support in advance.
Regards,
Ken