This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS544B20 Iout measurement accuracy

Other Parts Discussed in Thread: TPS544B20

I tested TPS544B20 Iout measurement accuracy with TPS544B20EVM and Fusion Digital Power Designer.
We measured actual output current by shunt resistor. The measurement result of our customer was on a same level although they used an ammeter. 

The result is following. The error was larger than datasheet characteristic(+/- 3A and +/- 15%).  Is this normal?
In order to we get datasheet accuracy, do we have to set "IOUT_CAL_OFFSET"?

Actual value                 Read value
0A                                  0.13A
2A                                  2.38A
4A                                  4.5A
6A                                  6.75A
8A                                  9.13A
10A                               11.94A
12A                               14.06A
14A                               17.63A
16A                               20.38A
18A                               22.38A
20A                               25.5A

Best Regards,
Kohei Sasaki