Hi,
I want to use the BQ24266 and I have several questions:
1) Is there a difference between sleep mode and hiZ mode (USB1,2,3 = '1') ?
2) what is the sleep mode current ?
3) ~ChG pin - Can I use this pin for logic condition as follows:
if ~Chg'= 1' then HiZ mode ?
4) What is the current consumption when no Vin is applied ? (Vin = 0V and only battery is working)