Hi, all
I have a question about external clock synchronization of TPS65400.
How many voltage is the min/max trip level of the RCLOCK_SYNC terminal?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all
I have a question about external clock synchronization of TPS65400.
How many voltage is the min/max trip level of the RCLOCK_SYNC terminal?
Best Regards,
You can refer to DS's description, the high voltage is better to 2.5V to 3.3V.
thanks!
"The typical trip level of the synchronization terminal is 1.5 V. To ensure proper
synchronization and to avoid damaging the IC, the peak-to-peak value (amplitude) should be between 2.5 V and
VDDA. The minimum duration of this pulse must be greater than 200 ns, and its maximum duration must be 200
ns less than the period of the switching cycle"