This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS50601-SP parallel connection

Hi,

I Need to supply an FPGA 0.9V/15A.

Can I connect 3 TPS50601 in parallel?

The dtasheet shows application of 2 component in parrale but I saw no comment on a connection of more than two...

If it is possible to connect 3 in parallel, a reference design would be greatly appreciated.

Regards,

Itai