Hi,
In the LM5088 datasheet:
1) EN Standby Threshold (VEN Rising) is typically 1.2V
2) EN Standby Hysteresis (VEN Falling) = 120mV.
The device I'm working with turns on @1.18V so the turn off voltage should be ~1.2V-120mv= 1.08V but in practice the device turns off @ ~1.12V
I don't "see" the 120mV hysteresis. To which voltage is the 120mV referenced to?