This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setting external MPPT of BQ25570 using VRDIV

Other Parts Discussed in Thread: BQ25570, BQ25504

Hello,

I am using the BQ25570 to harvest from RF source. The RF source has a non-continuous carrier wave, so if the MPPT sampling occurs when there is no transmission a wrong value is used. Since there is no way to disable the MPPT function I want to set a fixed voltage (although tunable by resistor ratio) at the VOC_SAMP port.

Since my design uses the BQ25570 as only power source, I would like to use the VRDIV port as reference voltage.  Is it possible to connect another resistive divider from VRDIV to GND, with the middle point connected to VOC_SAMP? If so, should I also obey the recommendation to keep the sum of the used resistors between 11 and 15 Megaohm? And is the voltage provided by VRDIV equal to VBIAS (=1.21V nominally) or should I calculate my reference using another expression?

Best regards,
Michel Jansen

  • VRDIV is not a constant reference voltage.  As shown in datasheet figure 40, it only has a voltage on it every 64ms for a brief time and that voltage varies.  bq25504, the core from which bq25570 was derived, can have MPPT sampling disabled.   

  • I am too far in my current design to switch to the BQ25504, but that would indeed be a solution.
    I have decided to connect it to VOUT with total sum of resistors 20 Megaohm (even though it is a kind of dirty fix).
    Thanks for your clarification anyway!