This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013B

Other Parts Discussed in Thread: BQ51013B

Hi, I wish to connect TS-CTRL directly to Microcontroller (NXP LPC12XX) to shut down BQ51013B instead of using EN1, EN2, because I have no PCB board space available. My question is, on BQ51013B data sheet, on page 25 is written that MAX low level voltage is 0,05 mV that is far lower than MAX low level voltage on micro controller output pin  (typical 0.4 V), could I go on or not on such solution?