Hello,
This is more or less addressed to Kevin LaRosa.
Looking through the TPS65086x EVM user guide (SLVUAH2), the CTL Inputs are OTP-configured as
CTL1=Controller enable (Buck1,2,6)
CTL2=converter enable (Buck 3 through 5)
CTL3=Sleep
CTL4=LDO Enable
CTL5=Load Switch Enable
CTL6=VTT Enable
Looking at the document you recently posted (Default OTP Settings.xslx) or OTP_Comparison_TPS650860_TPS650864x.xslx I see a different use of the CTL Registers:
Alternate Voltage Pin
BUCK1 CTL6 (masked)
...
BUCK4 CTL3
Can you please clarify? Does the EVM have different OTP programming than the regular '860s?
Another question: Is there a chance for OTP programming at the customer's site? Example scenario: Initally the PMIC is blank and completely inactive. Then program the necessary settings via I2C, verify them, OTP-progam them and start Operation.
Regards
Guenter