Perhaps this is a dumb question, but I am confused about the case of detecting a standard downstream port. This is from reading the datasheet, not from actual measurements.
The bq24295 datasheet seems to say that once it detects a SDP via primary detection, it decides it can pull 500mA for charging the battery. The USB specs (for 2.0 and earlier at least) says that powered devices can only pull 100mA until after they are enumerated and granted the additional power. Given that the bq24295 does not enumerate, how can it legally pull 500mA?
Have I misinterpreted the bq24295 datasheet, or the USB specs, or is there something I am missing (like you don't need to really pay attention to the 100mA current limit) or what?
Thanks in advance for a little clarity.
Hedley