This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1834J

Other Parts Discussed in Thread: TL1451

Hello,

I am having difficulty locating the Temperature Stability for this Linear Regulator on the data sheet. Could anyone tell me what the thermal specs are for the UC1834J?

  •  

    Hello Jesus

    This is a very versatile part that can be used in many configurations.  The actual power that is dissipated in the part would of course depend on the actual current draw from all ports in a given application summed together.  Once the power  across the part is calculated you will need the thermal resistance or derating factor to make sure that the package does not over heat - I think that this is what you are asking for?

    Fortunately, package thermal characteristics are not part dependant.  I found this in formation in the data sheet for the TL1452, where on page 3 you will find the derating information that I believe that you are looking for (for the J package).

    Regards

    Bill

  • Hello Bill,

     

    Yes I am looking for the thermal resistance. I understand that the thermal resistance will vary depending on the application. But I am trying to find the general min and max of that resistance, without taking into effect the application.

    I hope this makes sense.

    Thank you,

    Jesus

  • Jesus,

    I think that the Derating Factor for the "J" package is a good general number to be used for thermal calculations - and note that the Derating Factor is the reciprocal of the Thermal Resistance, theta_ja, between the ambient air temperature and the worst case semiconductor junction temperature. And so, based on the data found in the TL1451 data sheet the theta_ja = 1/Derating Factor = 1/11mW/degC = 90.9degC/Watt.  I apologise for any mis communication. 

    I find that thermal information is notoriously unsatisfying - especially "theta_ja" which is so dependant on the size of the copper area to which the part is attached. At Texas Insturments the amount of copper is in accord with some JEDEC standard PCB layout. But it is worth noting that the theta_ja does vary with the amount of copper area attached but probably less so for a leaded part with no heat tab.  Also note that a good estimate for thermal resistance to the top center of the package, Theta_jc, is approximately 60% of the theta_ja value. 

    (The worst case junction temperature is Tj=Tambient+(Theta_ja*Pd).  The junction temperature is determined by the ambient temp, Tambient, the thermal resistance, Theta_ja, and the dissipated power in the part, Pd.)

    Regards

    Bill

     

  • Hello Bill,

    We tested the parts at different temperatures with an voltage of 2V, the results we not consistent to that of the "J" package for the TL1451 specs. At -25 to -45 degrees the stability of the IC was very inconsistent, as for the 25 to 125 degrees the IC stayed stable without major fluctuation.

     

    Could you explain the reason behind the instability of the test in cold temperatures?

     

     

    Thank you,

     

    Jesus