I am going to use TPS65131 to generate both positive and negtive power supplies with single +5V input. I were confused when I had a look of the datasheet to find out what input range and output range are available. On page 4, section 6.3 it is specified that the minimum positive voltage us input voltage plus 0.5 Volt. But, on page 17, in figure 21, the output is +5Volt and the input can reach 5 volt even higher with good efficiency. Can this device output +/- 5V with a single 5V input?